• No : 23733
  • Release Date : 2018/09/19 17:16
  • Print

Movement of contact

How does the output contact behave during normal operation and when voltage drops?
Category : 

Answer

This relay uses the input voltage at the VT secondary side (P1-P2) as the relay control power source. When a rated voltage is input, b contact side of the contact will open. If voltage drops, with the settled operation time, b contact side will close.
Product Name
Protection Relay
Series
MELPRO-A Series