• No : 24774
  • Release Date : 2019/02/27 15:34
  • Print

Terminal blocks for the MELSEC-F series

Are the terminal blocks for the MELSEC series removable?
Category : 

Answer

Whether the terminal block is removable or not differs depending on the series. Types of the terminal blocks for the MELSEC-F series main units are as follows.
Note that when replacing a terminal block with another terminal block, they need to be the same model.
・ FX1S/3S series: Not removable
・ FX1N/FX3G series: Removable
・ FX2N/FX3U series: Removable except for 16-pin terminal block
Product Name
FX1S, FX1N, FX3S, FX3G, FX2N, FX3U
Product Category
Main unit
Series
MELSEC-F series