• No : 24777
  • Release Date : 2019/02/27 15:57
  • Print

Setting day of the week when using the TWR instruction (FX3 series)

Is day of the week automatically set in the FX3 series when date is written by using the TWR instruction?
Category : 

Answer

Day of week is automatically set.
When data written to the data register for storing day-of-the-week data is within the setting range (K = 0 to 6), the day of the week to be set for a clock is automatically corrected in accordance with the date.
Day of week setting values: 0 (Sunday) to 6 (Saturday)
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit
Series
MELSEC-F series