When trying to write a program to a programmable controller on which EEPROM and flash ROM are installed, an error (error code: 6772 "Memory cassette is write protected.") occurs and the program cannot be written to the programmable controller.
A memory cassette has a PROTECT switch to prevent a program from being overwritten in EEPROM and flash ROM.
When this switch is on, writing of the program is prohibited.