FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Support of the DHCP (Dynamic Host Con...
Back
No : 24870
Release Date : 2019/04/15 08:05
Print
Support of the DHCP (Dynamic Host Configuration Protocol) function by the FX3U-ENET-ADP (for Ethernet communications)
Does the FX3U-ENET-ADP support the DHCP function?
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
The FX3U-ENET-ADP does not support the DHCP function. Set the fixed IP address using the parameter setting of GX Works2. On GX Works2, select "Parameter" and "PLC Parameter". Click the "Ethernet Port Setting" tab, and set the fixed IP address.
Product Name
FX3U-ENET-ADP
Product Category
Network/Communication
Series
FX3S, FX3G, FX3GC, FX3U, FX3UC