• No : 24899
  • Release Date : 2019/04/15 11:30
  • Print

Thickness of ground wire

What should be the thickness of the ground wire?
Category : 

Answer

The thickness of wire should be 2 square millimeters or more, and class D grounding (grounding resistance: 100 Ω or less) should be performed.
Product Name
MELSEC-F Series
Product Category
FX1S,FX1N,FX2N,FX3S,FX3G,FX3U
Series
Main Unit