• No : 24912
  • Release Date : 2019/04/17 11:39
  • Print

Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3U series

How many FX3U-ENET-ADPs can be connected to the FX3U series?
Category : 

Answer

One FX3U-ENET-ADP can be connected at the last stage (left end) of adapters for the FX3U series.
*The FX3U-ENET-ADP is a communication special adapter and occupies one communication channel. Therefore, when the FX3U-ENET-ADP is connected to the FX3U series, another expansion board/special adapter (including the FX3U-8AV-BD/FX3U-CF-ADP) can be used.
Product Name
MELSEC-F Series
Product Category
FX3U
Series
Main Unit