Whether the positioning parameter is used or the extension positioning parameter is used can be selected in BFM#32 (positioning parameter selection). Select BFM#0 to #15 for K0 and select BFM#33 to #52 for K1. * When the parameter in BFM#32 is changed during operation, this change becomes valid from the next operation.