• No : 24917
  • Release Date : 2019/04/17 11:40
  • Print

Parameter setting of FX3U-1PG

When setting parameters, such as maximum speed and pulse rate, in the FX3U-1PG, there are two types of parameters. Which parameter will be used?
Category : 

Answer

Whether the positioning parameter is used or the extension positioning parameter is used can be selected in BFM#32 (positioning parameter selection). Select BFM#0 to #15 for K0 and select BFM#33 to #52 for K1. * When the parameter in BFM#32 is changed during operation, this change becomes valid from the next operation.
Product Name
MELSEC-F Series
Product Category
FX3U,FX3UC
Series
Positioning Control