For communications using MELSOFT connection, such as GX Developer, GX Works2, GOT1000, and MX Component, up to two personal computers can be used.
In addition, up to two lines can be connected in combination of sending or receiving data in the fixed buffer (non-protocol) communication.