• No : 24925
  • Release Date : 2019/04/17 11:42
  • Print

Using a fixed latched (battery backed) type device as a general type device

How can I use a fixed latched (battery backed) type device as a general type device?
Category : 

Answer

Clear the required area with the ZRST instruction by using the initial pulse when the programmable controller is set to RUN. To clear all the latched type devices, turn on M8032 (latch memory all clear).
Product Name
MELSEC-F Series
Product Category
FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Series
Main Unit