FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Adding two channels of the RS-232C port in the FX3G series
Back
No : 24926
Release Date : 2019/04/17 11:42
Print
Adding two channels of the RS-232C port in the FX3G series
I would like to add two channels of the RS-232C port in the FX3G series. How can I add the communication expansion boards and adapters?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Main Unit
Answer
Select the 40-point or 60-point type FX3G series main unit. In this case, two FX3G-232-BDs can be connected. When FX3G-CNV-ADP is used, an FX3U-232ADP can be used instead of an FX3G-232-BD.
Product Name
MELSEC-F Series
Product Category
FX3G
Series
Main Unit