• No : 24931
  • Release Date : 2019/04/17 11:43
  • Print

Overwriting a current value with the high-speed counter comparison instruction

The output contact is not set by overwriting the current value with the MOV instruction while using the high-speed counter comparison.
Category : 

Answer

The output contact is activated according to the change of the current value register along with the counting input. Therefore, the value changed by executing the MOV instruction is not set before the next count input is received.
Product Name
MELSEC-F
Product Category
FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Series
Main Unit