• No : 24948
  • Release Date : 2019/04/18 14:27
  • Print

Station number setting in the "PLC System(2)" tab of PLC Parameter setting on GX Developer when non-protocol communication is performed

To perform the non-protocol communication with the FX programmable controller, how should I specify the station number setting in "PLC System(2)" of PLC parameter setting on GX Developer?
Category : 

Answer

The station number setting is not required for non-protocol communication.
Product Name
MELSEC-F Series
Product Category
FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Series
Main Unit, Network/Communication