FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Using the FX3U-16CCL-M and FX2N-16CCL...
Back
No : 24954
Release Date : 2019/04/18 14:28
Print
Using the FX3U-16CCL-M and FX2N-16CCL-M together
Is it possible to add the FX3U-16CCL-M and FX2N-16CCL-M together to one main unit?
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
No, they cannot be added together. Only one FX3U-16CCL-M can be connected to one main unit. Multiple FX2N-16CCL-Ms can be connected to one main unit (depending on the programmable controller series and the number of other special extension units).
Product Name
MELSEC-F Series
Product Category
FX3G,FX3GC,FX3U,FX3UC
Series
Network/Communication