• No : 24974
  • Release Date : 2019/04/23 07:20
  • Print

Setting for installing a memory cassette

Are any settings required for installing a memory cassette to the programmable controller?
Category : 

Answer

When the programmable controller is powered on after a memory cassette is installed, the memory cassette is automatically recognized. After the memory cassette is installed, it is separated from the built-in memory of the programmable controller, and peripherals read/write data only from/to the optional memory.
Product Name
MELSEC-F Series
Product Category
FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Series
Main Unit