Usually, unit number of the first special function unit/block is "K0". However, when the main unit is FX3UC-32MT-LT(-LT2), the unit number "K0" is assigned to the built-in master for CC-Link/LT. Specify "K1" for the unit number of the first special function unit/block.