• No : 38041
  • Release Date : 2021/02/25 17:54
  • Print

Pulse magnification setting of EMU4-PX4(Pulse Input Unit)

How to set the pulse conversion rate of EMU4-PX4(Pulse Input Unit) and the pulse factor of EcoWebServerIII? Also, how to deal with one-cycle operation(when the value exceeds the data range and returns to 0)?
Category : 

Answer

Match the setting values with EMU4-PX4 and EcoWebServerIII.
No need to consider one-cycle operation because it is automatically calculated in EcoWebServerIII.
Product Name
Energy Saving Data Collecting Servers, Energy Measuring Units
Series
EcoWebServerIII, EcoMonitorPlus