• No : 39292
  • Release Date : 2023/02/13 15:37
  • Print

Regarding clearing error with SM50

Does turning on SM50 clear the error code stored in SD0?
Category : 

Answer

It is cleared by eliminating the cause of the error during detection and turning on SM50.
For the error codes that can be cleared on the SM50, refer to the manual below.
MELSEC iQ-F FX5 User's Manual (Application)
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series