• No : 39346
  • Release Date : 2023/02/15 10:05
  • Update : 2024/04/25 10:10
  • Print

Regarding Simple CPU communication function connection between CC-Link IE Field Network Basic masters within 1 network

Is it possible to perform data-link between FX5 CPU modules using CC-Link IE Field Network Basic within a single network using the Simple CPU communication function?
Category : 

Answer

It cannot. Because there will be two CC-link IE field network Basic master stations in a network.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Network/Communication
Series
MELSEC iQ-F Series