• No : 39351
  • Release Date : 2023/02/15 13:08
  • Update : 2024/08/19 09:54
  • Print

Regarding the differences between Latches (1) and (2)

Answer

Whether the latch range is set by default is different.
・Latch (1) — Latch range is set by default. This can be changed at any time.
・Latch (2) — No latch range is set by default. This is optional.
 
The latch range can be set between latch (1) and latch (2). Make sure that the ranges do not overlap.
 
Also, the range to clear from [Online] -[CPU Memory Operation] in GX Works3 differs.
・To clear devices outside the latch range.
・To clear the range of device outside the latch range + latch (1).
・To clear the device outside the latch range + the range of the latch (1) + the range of the latch (2).
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Engineering Software
Series
MELSEC iQ-F Series