• No : 39356
  • Release Date : 2023/02/15 13:03
  • Print

Regarding changing the current address (user unit, pulse unit)

Is it possible to change the current address (per user, per pulseuser unit, pulse unit) of the built-in positioning function?
Category : 

Answer

It can be changed.
It is now possible to write to the address (user unit, pulse unit) by the DHCMOV command. However, writing is disabled during positioning operations.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Motion/Positioning
Series
MELSEC iQ-F Series