(1)Whether or not networks can be mixed on the same trunk line is different.
CC-Link IE TSN allows network mixing on the same trunk line. When using a CC-Link IE field network and TCP/IP communication, you must wire each network separately.
(2)The communication method is different.
The CC-Link IE TSN is a time-synchronized method, and the CC-Link IE field network is a token-passing method.