• No : 40034
  • Release Date : 2023/08/24 15:39
  • Print

Regarding Cloud Connectivity

Is it possible to connect to the cloud with the iQ-F series?
Category : 

Answer

It is possible to connect to the cloud: MQTT broker (server) using the MQTT communication function of FX5-ENET.
The MQTT communication function is supported in the following versions.
・Hardware serial number: 234 **** or later
・Firmware version 1.200 or later
Product Name
FX5-ENET
Product Category
Network/Communication
Series
MELSEC iQ-F Series