There are three QoS levels and FX5-ENET is also supported.
・QoS0 - The message is sent only once from the source client.
Messages are not guaranteed to arrive at the destination.
・QoS1 - The message is retransmitted until it reaches the destination client.
Duplicate messages may arrive at the destination.
・QoS2 - Messages are delivered so that they reach the destination client only once.
*The higher the QoS level, the more accurate the message and the higher the quality, but the higher the number of communications, the higher the communication load.