The following points are different for the iQ-F series.
・All output disabled flag (SM8034)
When SM8034 is ON, the all output disabled flag is given priority, so all output terminals are turned OFF regardless of forced ON/OFF registration, and only the forced ON/OFF is reflected on the output device.
・Non-latch memory all clear (SM8031)
If SM8031 is ON, forced ON/OFF will not be reflected.
・Memory hold stop (SM8033)
If SM8033 is ON, forced ON/OFF will not be reflected.