• No : 44336
  • Release Date : 2024/03/20 13:28
  • Print

Regarding use of the FTP Server Auto Transfer Function with Other Functions

Please let me know if there are any precautions when using the FTP server auto transfer function with other functions.
Category : 

Answer

Be careful when using the FTP server auto transfer function in combination with the following functions.
・FTP client (FTPPUT instruction)
 The function executed later is placed in the transfer waiting state until the function executed earlier is completed.
・GX LogViewer
 When a transfer-enabled file on the SD memory card is being accessed from GX LogViewer, it is placed in transfer standby. If the transfer wait status continues, file transfer fails.
 When accessing from GX LogViewer, access the locally transferred file.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series