The MQTT communication function cannot publish and subscribe at the same time.
A program for the MQTT communication function is created using FB, but it cannot be executed at the same time because an Ethernet Module is used in FB and the following restrictions are imposed.
Restrictions
・Do not concurrently execute this FB and any other Ethernet module dedicated instruction or any FB including an Ethernet module dedicated instruction.