The FX5-CNV-IF is an additional cable type.
・FX5U/FX5UJ CPU Modules are supported.
・Used to connect an extension connector type module to an extension cable type module.
Example:FX5U-32MR/ES + FX5-CNV-IF + FX5-C16EX/D
The FX5-CNV-IFC is an additional connector type.
・The FX5UC CPU module supports it.
・Used to connect an extension cable type module to an extension connector type module.
Example:FX5UC-32MT/D + FX5-CNV-IFC + FX5-16EX/ES