• No : 44366
  • Release Date : 2024/03/27 16:19
  • Print

Regrading using the Positioning Function with a Relay-Output Type FX5 CPU Module

Can the positioning function be used by High-speed pulse I/O module : FX5-16 ET/ES-H to the relay output type FX5 CPU Module?
Category : 

Answer

High-speed pulse I/O module : The FX5-16 ET/ES-H can be added regardless of the output type of the CPU Module, and the positioning function can be used with the relay output type FX5 CPU Module.
*FX5S CPU Modules are excluded.
Product Name
FX5U,FX5UC,FX5UJ,FX5S
Product Category
CPU Module, Engineering Software
Series
MELSEC iQ-F Series