• No : 44651
  • Release Date : 2025/03/18 10:22
  • Print

Regarding number of CH of CPU Module built-in Heating/Cooling PID control

How many channels can the built-in Heating/Cooling PID control function of the CPU Module support?

Category : 

Answer

The CPU Module's built-in Heating/Cooling PID control function supports up to 16 channels.
The following firmware versions are required in order to use it.

FX5U/FX5UC: 1.320 or later
FX5UJ: 1.080 or later
FX5S: 1.040 or later
GX Works3 1.110Q and later

Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module,Analog
Series
MELSEC iQ-F Series