• No : 44877
  • Release Date : 2025/03/18 10:30
  • Print

Regarding CC-Link IE field network support of FX5 CPU module built-in Ethernet

Does the FX5 CPU module built-in Ethernet support the CC-Link IE field network?

Category : 

Answer

The built-in Ethernet on the FX5 CPU module does not support CC-Link IE field networks. 

If you use a CC-Link IE field network, add an FX5-CCLIEF.

*The FX5-CCLIEF does not support the master function. Supports intelligent device stations.

Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Network/Communication
Series
MELSEC iQ-F Series