• No : 45244
  • Release Date : 2025/10/22 17:03
  • Print

Controlling the GOT buzzer

Answer

The GOT buzzer can be sounded intentionally. 
Set the system information in the screen design software. 
The buzzer can be output using the system information (read device). 
• Buzzer Three-shot Output signal (System signal 1-1.b8)
• Buzzer Output signal (System signal 1-1.b14)
• Buzzer One-shot Output signal (System signal l 1-1.b15)

◆ For GT Designer3 (GOT2000) Version 1
1. Set the system information read device. 
 Select [Common] - [GOT Environmental Setting] - [System Information], and then select [Use System Information]. 
 Set a device for [System Signal 1-1]. 
2. Turn on b8, b14, or b15 of System signal 1-1 using the GOT or sequence program. 
 The buzzer is output.

* The buzzer volume cannot be changed.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (buzzer output)
Series
GOT2000 Series, GOT3000 Series