Where should I enter the IP address of the PLC when connecting the GOT to a PLC via Ethernet?
When connecting the GOT to a PLC via Ethernet, set the IP address of the PLC in the screen design software.
◆ For GT Designer3 (GOT2000) Version 1
Select [Common] → [Controller Setting] to display the [Controller Setting] dialog.
(1) Set [Manufacturer] and [Controller Type] of the device being connected and set [I/F] to "Ethernet: Multi".
(2) Enter the IP address of the device being connected in [Connected Ethernet Controller Setting].
When using the "New" wizard, configure the settings on the setting screen after the wizard has closed.