What gestures are available for the document display function?
The following gestures are available for the document display function.
• Swipe: Scroll or change the page in the direction swiped (eight directions)
• Pinch in: Zoom out (25% to 400%)
• Pinch out: Zoom in (25% to 400%)
*1: For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.