- No : 20861
- Release Date : 2018/08/22 16:24
-
Print
Operation mode switch of the FR-A800/F800
Pr.79 is set to "0", however, the external operation is not switched to the PU operation with the PU/EXT button. What can be its cause?
- Category :
-
Answer
When Pr.551 is set to "3" (Command right to the USB connector at the PU operation), or when the USB is connected, the operation is not switched.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800