- No : 21018
- Release Date : 2018/08/22 16:25
-
Print
Control power supply
Can I use separate power supply for the control circuit with the 24 V external power supply?
- Category :
-
Answer
Turning ON the main circuit power stops the 24 V external power supply operation and enables the normal operation. Therefore, the separate power supply cannot be used with the 24 V external power supply. Use the power supply terminal for control circuit (R1/L11, S1/L21) for using the separate power supply. (For the detail, refer to the Instruction Manual.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800