- No : 21277
- Release Date : 2018/08/22 16:26
-
Print
Input phase loss
Can I change the detection time 1 s of the input phase loss?
- Category :
-
Answer
The detection time 1 s cannot be changed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700