• No : 21301
  • Release Date : 2018/08/22 16:26
  • Print

RS-485 communication

I want to operate the inverter in RS-485 communication.
I have input forward rotation command with the communication, but the "RUN" LED on the panel blinks and the inverter does not operate.
What are the possible causes for this?
Category : 

Answer

Blinking of the "RUN" LED on the panel suggests that the frequency command may not be input.
Create a frequency setting data as for the forward rotation command and send it to the inverter.
For how to format the data, refer to the Instruction Manual (Applied).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700