- No : 21303
- Release Date : 2018/08/22 16:26
-
Print
FR-PA07
When Pr.79 (Operation mode) is set to "3", and using the option FR-PA07 and external terminals, does the RUN key on the FR-PA07 work?
- Category :
-
Answer
When Pr.79 is set to "3", since the start command is in the External operation mode, the RUN key of FR-PA07 does not work.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700