- No : 21312
- Release Date : 2018/08/22 16:26
-
Print
Connection cable of FR-Configurator
I want to communicate with FR-Configurator (FR-SW3-SETUP-WJ) using the USB connector.
Is the Mini-B indicates the standardized Mini-B connector?
- Category :
-
Answer
It is the standardized Mini-B connector.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700