- No : 21315
- Release Date : 2018/08/22 16:27
-
Print
Printing files saved in the previous version of FR-Configurator
Can I print the parameter file of FR-SW3 using FR-SW2 in FR-Configurator (FR-SW3-SETUP-WJ) Ver.2.00?
- Category :
-
Answer
The parameter file of FR-SW3 cannot be printed using FR-SW2.
The latest version of FR-SW3 can be downloaded from the Mitsubishi Electric FA Global Website. Update FR-SW2 to FR-SW3.
Match the version of FR-Configurator when using it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700