- No : 21316
- Release Date : 2018/08/22 16:27
-
Print
Printing (character size) of FR-Configurator
The parameter list is printed in small characters in FR-Configurator (FR-SW3-SETUP-WJ) Ver.2.00.
Can I print it in big characters as with FR-SW1 and FR-SW2?
- Category :
-
Answer
The size of the fonts are bigger to make it easy to read in Ver.2.01 of FR-Configurator (FR-SW3-SETUP-WJ).
Download the latest version from the Mitsubishi Electric FA Global Website for update.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700