- No : 21338
- Release Date : 2018/08/22 16:27
-
Print
Countermeasure against noises
Can I change the countermeasure against the inverter noise by changing the parameter?
- Category :
-
Answer
Yes.
The carrier frequency can be decreased by the setting of Pr.72 (PWM frequency selection).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700