- No : 21342
- Release Date : 2018/08/22 16:27
-
Print
Wiring the terminal
I use the 24 VDC power supply of the terminal PC with a 24 VDC relay across the terminals PC and RUN and terminals across SD and SE shortened.
Is there any problem with the wiring?
- Category :
-
Answer
There is no problem with the wiring.
Keep the rating (24 VDC, 0.1 A) of the terminal PC.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700