- No : 21345
- Release Date : 2018/08/22 16:27
-
Print
Output frequency
What is the upper limit of the inverter output frequency (Hz) in the initial setting?
- Category :
-
Answer
In the initial setting, it is set to 120 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700