• No : 21345
  • Release Date : 2018/08/22 16:27
  • Print

Output frequency

Answer

In the initial setting, it is set to 120 Hz.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700