• No : 21347
  • Release Date : 2018/08/22 16:27
  • Print

Frequency setting

I want to change the output frequency. Is it changed by changing the setting of Pr.1 (Maximum frequency)?
Category : 

Answer

The output frequency is not changed by the maximum frequency setting.

It can be changed by the following methods.

- Set the frequency on the operation panel.
- Set the frequency (terminal 10-2-5 connection) with the potentiometer (frequency setting potentiometer).
- Set the frequency (terminal 4-5 connection) with the current output device (4 DC to 20 mA).
- Change the frequency to the one set in the parameter in advance by turning ON/OFF the switch connected to the terminal. (Multi-speed setting: terminal RH, RM, RL etc.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700