• No : 21350
  • Release Date : 2018/08/22 16:27
  • Print

Easy setting mode

When I tried to change Pr.79 (Operation mode selection) in the easy setting mode to input the start command and frequency command on the operation panel, "HOLD" was displayed.

How can I clear it?
Category : 

Answer

If "HOLD" is displayed, the key lock mode enabled.

Press the "MODE" key for two seconds.

Then, change the setting of Pr.79 to "1".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700