• No : 21361
  • Release Date : 2018/08/22 16:27
  • Print

FR-PA07

Is the mounting screw supplied with the optional FR-PA07?

Do I have to use a nut for the installation?
Category : 

Answer

The mounting screw is not supplied. The mounting screw is supplied with the operation panel.
Open the screw hole according to the dimension. (The M3 screw is used.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700